Drive_Inputs_Level
| Index.Sub | 2200.1H | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Data Type | Unsigned16 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Access | Read/Write | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| PDO Mappable | No | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Unit | -- | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Range |
0 ÷ FFFFH | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Default Value | -- | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Store Supported | Yes | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Description |
This object is used to set drive digital inputs working level for functionality defined with bit#0, bit#1 and bit#2 of Drive_Working_Settings object.
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Notes |
|
Bit Explanation:
Forward_Limit_Switch_Level(1):
-
When this bit is set to (1), the drive will consider the Forward Limit Switch intervention when the corresponding digital input (see Drive_Inputs_Setting object) will close.
-
When this bit is reset to (0) the drive will consider the Forward Limit Switch intervention when the corresponding digital input (see Drive_Inputs_Setting object) will open.
Backward_Limit_Switch_Level(1)
-
When this bit is set (1) the drive will consider the Backward Limit Switch intervention when the corresponding digital input (see Drive_Inputs_Setting object) will close.
-
When this bit is reset (0) the drive will consider the Backward Limit Switch intervention when the corresponding digital input (see Drive_Inputs_Setting object) will open.
Fast_Stop_Level(2) :
-
When this bit is set (1) the drive will consider the Fast Stop input intervention when the corresponding digital input (see Drive_Inputs_Setting object) will close.
-
When this bit is reset (0) the drive will consider the Fast Stop input intervention.
-
When the corresponding digital input (see Drive_Inputs_Setting object) will open.